News Center | Press Release

TDK presents next-generation technologies at CEATEC JAPAN 2017

  • Booth theme: “Technologies & Solutions for a Connected Society”
  • Location and booth number: Hall 6, D353
TDK presents next-generation technologies at CEATEC JAPAN 2017

September 26, 2017

TDK Corporation will be exhibiting at CEATEC JAPAN 2017, October 3 to 6, at the Makuhari Messe in Chiba City.

Under the theme “Technologies & Solutions for a Connected Society” TDK will be exhibiting next-generation technologies that support lifestyles supported by loT (Internet of Things), AI (Artificial Intelligence) and VR (Virtual Reality). The booth will feature sensors, energy units and solutions in four different zones:

  1. Demonstration Zone
    Demonstrations of VR, biosensors, a robotic arm, and more
  2. Sensor Zone
    Demonstrations of magnetic, temperature, pressure and sound sensors
  3. Solutions Zone
    Motion sensors, biosensors (Silmee™), IoT solution examples, EDLC, PV and SESUB solutions
  4. Energy Units & Next-Generation Electronic Components Zone
    Wireless power transfer, PiezoHapt™ and PowerHap™ actuators with haptic feedback and electronic components such as MLCCs, inductors and EMC components

Visitors can experience TDK's most advanced technologies, including a demonstration of a movable robotic arm that is controlled via a remote control using TDK’s TMR angle sensors, imitating human arm movement. In addition, TDK will also present a wide range of products and technologies, such as the its 50 W-class wireless power transfer system, which will be presented for the first time, and the demonstration of different vibrations using TDK’s super-thin PiezoHapt™ actuator.

TDK is looking forward to welcome you at its booth!

A preview of the booth can be found at TDK’s Global website: https://product.tdk.com/info/en/news/event/2017ceatec.html

Glossary

 
  • EDLC: Electric double-layer capacitor, a special type of capacitor with the intermediate characteristics of a standard capacitor and battery (secondary battery)
  • PV:Photovoltaic
  • SESUB:Semiconductor embedded in substrate, in which a thinned IC is embedded into a substrate and can be mounted with various electronic components
  • TMR:Tunnel magnetoresistance. Of all magnetic field sensors, TMR sensors offer the greatest sensitivity.
 

Locationand booth number

Devices & Software Area, Hall 6, D353

About TDK Corporation

TDK Corporation is a leading electronics company based in Tokyo, Japan. It was established in 1935 to commercialize ferrite, a key material in electronic and magnetic products. TDK's portfolio includes passive components, such as ceramic, aluminum electrolytic and film capacitors, ferrites and inductors, high-frequency products, and piezo and protection components, as well as sensors and sensor systems and power supplies. These products are marketed under the product brands TDK, EPCOS, InvenSense, Micronas, Tronics and TDK-Lambda. TDK's further main product groups include magnetic application products, energy devices, and flash memory application devices. TDK focuses on demanding markets in the areas of information and communication technology and automotive, industrial and consumer electronics. The company has a network of design and manufacturing locations and sales offices in Asia, Europe, and in North and South America. In fiscal 2017, TDK posted total sales of USD 10.5 billion and employed about 100,000 people worldwide.

Contacts for media

Region Contact Phone Mail
Japan Mr. Yoichi OSUGA TDK Corporation
Tokyo, Japan
+81 3 6852-7102 TDK.PR@tdk.com