Technology

TDK Components Used in the Porsche 99X Electric

To maximize the performance of the Porsche 99X Electric’s powertrain and ensure unwavering reliability in the most grueling racing environments, TDK’s cutting-edge components play a vital role. Below is an introduction to our products and their contributions to the latest "GEN3 Evo" model.

※ Click on a product in the image to view more details.

※ Tap a product from the list to view more details.

Multilayer Ceramic Chip Capacitors (MLCCs)

Essential for circuit design, these components stabilize the power supply by smoothing voltage fluctuations.
In the Porsche 99X Electric, they ensure the efficient and stable operation of the inverter, supporting consistent power output throughout the race.
Product Details

Chip Beads

These components suppress high-frequency electrical noise generated within the inverter.
In the Porsche 99X Electric, they protect precise control signals from noise and improve Electromagnetic Compatibility (EMC), thereby increasing the accuracy of the vehicle's entire electronic control system.
Product Details

Common Mode Filters

These filters reduce common-mode noise caused by inverter switching, both internally and across other vehicle systems.
In the Porsche 99X Electric, they enhance the reliability of the inverter while preventing radio interference with other electronic devices, contributing to the stable operation of the entire vehicle.
Product Details

Motion/Inertial Sensors

These sensors precisely detect vibrations and movements related to the inverter and vehicle dynamics.
In the Porsche 99X Electric, they enable precise monitoring of the powertrain's behavior, supporting optimal machine setup and sustained performance in the extreme conditions of a race.
Product Details

SMD/SMT Inductors (Coils)

Inductors ensure smooth current flow and reduce ripple current within the inverter’s Printed Circuit Boards (PCBs).
In the Porsche 99X Electric, they enhance the reliability of the inverter and prevent unwanted electrical interference, maintaining the integrity of electronic systems during intense circuit driving.
Product Details

What is the Porsche 99X Electric (GEN3 Evo)?

The GEN3 Evo is Porsche’s state-of-the-art electric racing car, making its debut in Season 11 (2024/25) of the ABB FIA Formula E World Championship.

Key Features:

  • Breathtaking Acceleration: Boasting a 0-100 km/h acceleration time of approximately 2.0 seconds, it delivers performance that surpasses even current Formula 1 machines.
  • First-ever All-Wheel Drive (AWD): The front motor engages under specific conditions—such as the start, qualifying, and during Attack Mode—enabling four-wheel drive performance.
  • Extreme Energy Efficiency: Motor efficiency exceeds 95%, with regenerative braking providing nearly half of the energy used during a race.
  • In-house Developed Core: Porsche Motorsport optimizes energy management by developing key components—including the pulse inverter, gearbox, differential, suspension, and control software—entirely in-house.

Porsche secured both the Teams’ and Manufacturers’ World Championship titles in the 2024/25 season with the Porsche 99X Electric. This vehicle also serves as a critical development platform, providing a feedback loop for Porsche’s most advanced EV technologies to be integrated into production models like the Taycan.

Partnership Insights

For us, Formula E is not just a race, but a laboratory where electrification technologies are refined to their absolute limits.
With the Porsche 99X Electric, energy efficiency, reliability, and precise control are all decisive factors for performance.
TDK’s electronic component technologies form a crucial foundation that enables the inverter and powertrain to operate reliably and deliver stable performance even under these extremely demanding conditions.
The technologies proven and refined on the racetrack will undoubtedly be carried over into future production electric vehicles.

Florian Modlinger

Director Factory Motorsport Formula E Porsche Motorsport