Press Release | May 19, 2026

Power management products: TDK expands micro POL power module portfolio for high-density AI edge systems

The actual appearance of the product differs from the image.
TDK logo is not stamped on the actual product.
  • Ultra-compact micro POL module FS3303 delivers 3 A in a 2.5 × 2.5 mm footprint with only 1.2 mm height, enabling high-density power for optical modules and AI edge systems
  • High efficiency up to 95% with operation up to +90 °C (and +125 °C with derating), supporting low-voltage rails from 0.4 V to 3.3 V for ASICs, SoCs, DSPs, and AI chipsets
  • Integrates controller, driver, MOSFETs, and inductor in TDK’s advanced 3D chip-embedded package, minimizing external components and maximizing board space savings

TDK Corporation (TSE: 6762) today announced the FS3303, the first member of a major expansion of its micro POL family of ultra‑compact, non‑isolated DC‑DC power modules for optical modules in AI edge systems and other space‑constrained designs. Despite its small footprint of just 2.5 x 2.5 mm and a height of only 1.2 mm, the FS3303 can deliver 3 A at ambient temperatures of up to +90 °C (up to +125 °C with derating) and boasts a peak efficiency of around 95%. The FS3303-0400-AL is in full production and is sampling at major distributors.

The FS3303 and the upcoming high‑performance point‑of‑load (POL) converter lineup spans 3 A to 80 A output across 0.3 V to 3.3 V rails. They enable next‑generation optical networking and AI accelerator platforms to push performance without sacrificing board space. An example is compact optical modules, which are scaling from 10 Gbit/s to 1.6 Tbit/s. The new portfolio delivers height profiles between 1.2 mm and 1.7 mm.

Engineered for low‑voltage rails, the FS3303 supports input voltages from 2.7 V to 6 V and output voltages from 0.4 V to 3.3 V. This makes it a versatile solution for ASICs, SoCs, DSPs, and emerging AI chipsets requiring tight regulation and high transient performance.

The FS3303 leverages TDK’s proprietary 3D chip‑embedded packaging technology, integrating the controller, driver, MOSFETs, and power inductor. This architecture minimizes external components and delivers a complete DC‑DC solution with exceptional area and height savings—ideal for next‑generation optical transceivers and edge AI modules.

Article assets

Contacts for regional media

R. HIGGELKE

Europe
TDK Electronics AG München, Deutschland
+49 89 54020 1378
ralf.higgelke@tdk.com

D. MARTIN

North America
TDK Electronics Inc. Woodbridge, NJ, USA
+1 732 906 4364
debbie.martin@tdk.com

C. DALL’AGNOL

South America
TDK Electronics do Brasil Ltda., Gravataí, Brazil
+55 51 3484 7158
candido.dallagnol@tdk.com

H. BAGHEL

India
TDK India Private Limited Noida, India
+91 12 04 50 58 42
himalaya.baghel@tdk.com

K. Xu

Greater China
TDK (Shanghai) Electronics Ltd. Shanghai, China
+86 21 2219 1598
Kathy.Xu@tdk.com

D. ITO

Japan
TDK Corporation Tokyo, Japan
+813 6778 1055
TDK.PR@tdk.com

About TDK Corporation

TDK Corporation (TSE:6762) is a global technology company and innovation leader in the electronics industry, based in Tokyo, Japan. With the tagline “In Everything, Better” TDK aims to realize a better future across all aspects of life, industry, and society. For over 90 years, TDK has shaped the world from within; from the pioneering ferrite cores to cassette tapes that defined an era, to powering the digital age with advanced components, sensors, and batteries, leading the way towards a more sustainable future. United by TDK Venture Spirit, a start-up mentality built on visions, courage and mutual trust, TDK’s passionate team members around the globe pursue better—for ourselves, customers, partners, and the world. Today, the state-of-the-art technologies of TDK are in everything, from industrial applications, energy systems, electric vehicles, to smartphones and gaming, at the core of modern life. TDK’s comprehensive, innovative-driven portfolio includes cutting-edge passive components, sensors and sensor systems, power supplies, lithium-ion and solid-state batteries, magnetic heads, AI and enterprise software solutions, and more—featuring numerous market-leading products. These are marketed under the product brands TDK, InvenSense, Micronas, Tronics, TDK-Lambda, TDK SensEI, and ATL. Positioning the AI ecosystem as a key strategic area, TDK leverages its global network across the automotive, information and communication technology, and industrial equipment sectors to expand its business in a wide range of fields. In fiscal 2026, TDK posted total sales of USD 16.6 billion and employed about 107,000 people worldwide.