News Center | Press Releases

EMC components: TDK offers multilayer chip beads with the industry's highest rated current of 8 A for power supply lines

  • Compatible with currents as high as 8 A
  • Saves space by reducing components and footprint
  • Highly reliable for use in high-temperature environments like automotive and industrial applications
press_01_250513_01.jpg
The actual appearance of the product differs from the image.
TDK logo is not stamped on the actual product.

May 13, 2025

TDK Corporation (TSE: 6762) has expanded its MPZ1608-PH series of large-current multilayer chip beads for automotive and commercial power supply lines (1.6 x 0.8 x 0.6 mm – L x W x H). Mass production of the product series began in May 2025.

These 1608-size chip beads for power supply lines achieve a rated current of 8 A, the industry’s highest value*. Chip beads are used as noise suppression components in power and signal circuits. In a circuit with a current of 8 A or more, usually two or more chip beads must be used in parallel. This has the disadvantage that the current is not evenly distributed between the ferrite beads. TDK’s new product simplifies the circuit structure because fewer components are required compared to conventional methods, and it improves the quality of power circuits.

The MPZ1608-PH series of products halves the component footprint in comparison with circuits using two conventional 1608-sized chip beads. Moreover, the highly reliable components with a specified operating temperature of up to +125 °C are designed to be used in high-temperature environments like automotive and industrial equipment applications.

With TDK’s proprietary materials and structural designs adapted to market needs, the company is committed to expanding its lineup of high rated current products in the automotive, industrial equipment, and consumer equipment areas. These chip beads will serve as EMC components contributing to the enhancement of the quality of power circuits.

*Source: TDK, as of May 2025

Glossary

  • EMC: electromagnetic compatibility

Main applications

  • Power circuit for different pieces of equipment: in-vehicle ECUs, power train, vehicle body control, automotive multimedia (telematics), base stations, PCs, servers, set-top box, smart grids, robots, smartphones, tablet devices, etc.

Main features and benefits

  • Compatible with large currents as high as 8 A
  • Reduces components and footprint
  • Highly reliable; can be used in high-temperature environments like automotive applications

Key data

Type Applications Impedance
[Ω] @100 MHz
DC resistance
[Ω] max.
Itemp
[A] max.
+85 °C
Itemp
[A] max.
+125 °C
MPZ1608SPH220ATAH0 Industrial 22 ± 7 0.004 8 5
MPZ1608SPH220ATDH5 Automotive 22 ± 7 0.004 8 5

About TDK Corporation

TDK Corporation is a world leader in electronic solutions for the smart society based in Tokyo, Japan. Built on a foundation of material sciences mastery, TDK welcomes societal transformation by resolutely remaining at the forefront of technological evolution. It was established in 1935 to commercialize ferrite, a key material in electronic and magnetic products. TDK’s comprehensive, innovation-driven portfolio features passive components such as ceramic, aluminum electrolytic and film capacitors, as well as magnetics, high-frequency, and piezo and protection devices. The product spectrum also includes sensors and sensor systems such as temperature and pressure, magnetic, and MEMS sensors. In addition, TDK provides power supplies and energy devices, magnetic heads, software and more. These products are marketed under the product brands TDK, EPCOS, InvenSense, Micronas, Tronics, and TDK-Lambda. TDK focuses on demanding markets in automotive, industrial and consumer electronics, and information and communication technology. The company has a network of design and manufacturing locations and sales offices in Asia, Europe, and in North and South America. In fiscal 2025, TDK posted total sales of USD 14.4 billion and employed about 105,000 people worldwide.

Downloads

Contacts for regional media

Region Contact Phone Mail
Japan Mr. Daiki Ito TDK Corporation
Tokyo, Japan
+813 6778-1055 TDK.PR@tdk.com
ASEAN Ms. Jiang MAN
Ms. Pei Lu LEE
TDK Singapore (Pte) Ltd.
Singapore
+65 6273 5022 tdk.asean-inquiry@tdk.com
Greater China Ms. Clover XU TDK China Co., Ltd.
Shanghai, China
+86 21 61962307 TDK.PR-CN@tdk.com
Europe Mr. Frank TRAMPNAU TDK Management Services GmbH
Duesseldorf, Germany
+49 211 9077 127 frank.trampnau@tdk.com
America Ms. Sara M. LAMBETH TDK Corporation of America
Plano, TX, USA
+1 972-409-4519 sara.lambeth@tdk.com