TDK wins Grand Prix in CEATEC AWARD 2022
October 18, 2022
TDK Corporation (TSE:6762) announces that TDK's i3 Micro Module has won the Grand Prix in the Smart x Industries Category in the CEATEC AWARD 2022.
The CEATEC AWARD marks its 12th anniversary this year. The CEATEC AWARD 2022 judging committee examines and evaluates, among the technologies, products, and services exhibited at CEATEC 2022, those entered by the exhibitors beforehand, assesses their academic and technological attributes, their marketability, potential and innovativeness and recognizes the particularly excellent among them.
TDK's i3 Micro Module, the winner of the award this year, is the world’s first wireless mesh sensor module featuring an embedded edge AI and contributes to the predictive maintenance of many types of equipment. i3 Micro Module is a compact and user-friendly autonomic sensing solution. It includes an industrial grade acceleration sensor and other features and is compact and easy to mount in the targeted equipment. The module is able to wirelessly facilitate predictive maintenance and automatically interconnect with other i3 Micro Modules, forming a wireless network, enabling it to establish a highly reliable system that covers a wide area. In addition, each module has embedded edge AI, which allows it to send only the information that is required for detecting conditions, and it boasts other features including low-power consumption and a long lifetime. As edge AI can process data to determine conditions inside the module, it ensures the confidentiality of the data. i3 Micro Module enables predictive maintenance by integrating AI and IOT and makes it possible to improve quality through the visualization of conditions, to improve productivity by minimizing the downtime caused by equipment whose operation is suspended and to reduce cost by extending the lifetime of the design.
i3 Micro Module received the award because of the committee highly evaluated realization of predictive maintenance, versatility, and marketability, such as high quality with industrial grade sensor, easy addition and deletion of sensors and other features of the module.
TDK aims to expand its growth opportunities and ultimately increase its corporate value following two major trends, DX (Digital Transformation) and EX (Energy Transformation).
By continuing to create valuable technologies and provide products, TDK will contribute to the realization of a sustainable society.
Products and awards
- Product: i3 Micro Module
- Award: Grand Prix in the Smart x Industries Category
About TDK Corporation
TDK Corporation is a world leader in electronic solutions for the smart society based in Tokyo, Japan. Built on a foundation of material sciences mastery, TDK welcomes societal transformation by resolutely remaining at the forefront of technological evolution and deliberately “Attracting Tomorrow.” It was established in 1935 to commercialize ferrite, a key material in electronic and magnetic products. TDK‘s comprehensive, innovation-driven portfolio features passive components such as ceramic, aluminum electrolytic and film capacitors, as well as magnetics, high-frequency, and piezo and protection devices. The product spectrum also includes sensors and sensor systems such as temperature and pressure, magnetic, and MEMS sensors. In addition, TDK provides power supplies and energy devices, magnetic heads and more. These products are marketed under the product brands TDK, EPCOS, InvenSense, Micronas, Tronics and TDK-Lambda. TDK focuses on demanding markets in automotive, industrial and consumer electronics, and information and communication technology. The company has a network of design and manufacturing locations and sales offices in Asia, Europe, and in North and South America In fiscal 2022, TDK posted total sales of USD 15.6 billion and employed about 117,000 people worldwide.
- Detailed product information is available at the following link:
https://www.tdk.com/en/featured_stories/entry_046-sensor-micro-module.html
Contacts for regional media
| Region | Contact | Phone | ||
|---|---|---|---|---|
| Japan | Mr. Yoichi OSUGA | TDK Corporation Tokyo, Japan |
+813 6778-1055 | TDK.PR@tdk.com |