EMC Products: TDK launches noise suppression filters for in-vehicle PoC
- Contributes to high-frequency isolation and control of radiation noise (0.7 - 2.4 GHz)
- Achieves 1000 Ω (at 900 GHz) or greater with the rated current of 400 mA at 125℃ in the 1005 form
- DC superimposition characteristics with good impedance
- AEC-Q200 compliant
December 15, 2020
TDK Corporation (TSE:6762) announces the launch of the MDF1005 series of noise suppression filters for in-vehicle PoC, used in applications such as ADAS circuits, BUS lines, telematics units, and more. Mass production will begin in December 2020.
The products in the MDF1005 series have good DC superimposition characteristics with impedance within the PoC high-frequency band, between 700 MHz and 2.4 GHz. The series is also optimal for the isolation of communication interfaces and noise control. Despite its small size, 1.0 millimeter long and 0.5 millimeter wide, the products in the series deliver 1000 ohms, or greater impedance with the rated current of 400 mA in environments reaching 125℃.
Using ferrite material with low loss within the high frequency band, the MDF series retains higher impedance at higher frequency when compared to general chip beads, and also controls impedance fluctuation during energization, meeting demands placed on PoC filters while demonstrating noise-controlling effects. The new filters are qualified in accordance with AEC-Q200.
TDK will continue working to expand the range of impedances to meet the noise control requirements of customers in various in-vehicle electronic devices.
Glossary
- PoC: Power over Coaxial, the transmission technology superimposing a signal line onto a power source line using a single coaxial cable.
Main applications
- ADAS circuit, BUS line, telematics unit (e.g. C-V2X, e-call)
Main features and benefits
- Contributes to high-frequency isolation and control of radiation noise (0.7 - 2.4 GHz)
- Achieves 1000 ohms (at 900 GHz) or greater with the rated current of 400 mA at 125℃ in the 1005 form
- DC superimposition characteristics with good impedance
Main features
Type | Impedance [Ω] typ. at 100 MHz | Impedance [Ω] typ. at 900 MHz | DC resistance [Ω] typ. | DC resistance [Ω] max. | Rated current [mA] max. |
---|---|---|---|---|---|
MDF1005GAD102ATD25 | 190 | 1000 | 0.53 | 0.69 | 400 |
About TDK Corporation
TDK Corporation is a world leader in electronic solutions for the smart society based in Tokyo, Japan. Built on a foundation of material sciences mastery, TDK welcomes societal transformation by resolutely remaining at the forefront of technological evolution and deliberately “Attracting Tomorrow.” It was established in 1935 to commercialize ferrite, a key material in electronic and magnetic products. TDK's comprehensive, innovation-driven portfolio features passive components such as ceramic, aluminum electrolytic and film capacitors, as well as magnetics, high-frequency, and piezo and protection devices. The product spectrum also includes sensors and sensor systems such as temperature and pressure, magnetic, and MEMS sensors. In addition, TDK provides power supplies and energy devices, magnetic heads and more. These products are marketed under the product brands TDK, EPCOS, InvenSense, Micronas, Tronics and TDK-Lambda. TDK focuses on demanding markets in automotive, industrial and consumer electronics, and information and communication technology. The company has a network of design and manufacturing locations and sales offices in Asia, Europe, and in North and South America. In fiscal 2020, TDK posted total sales of USD 12.5 billion and employed about 107,000 people worldwide.
Downloads
- Further information on the products can be found under
https://product.tdk.com/info/en/catalog/datasheets/suppression-filter_automotive_mdf1005_en.pdf.
Contacts for regional media
Region | Contact | Phone | ||
---|---|---|---|---|
Japan | Mr. Yoichi OSUGA | TDK Corporation Tokyo, Japan |
+813 6778-1055 | pr@jp.tdk.com |
ASEAN | Ms. Jiang MAN Ms. Pei Lu LEE |
TDK Singapore (Pte) Ltd. Singapore |
+65 6273 5022 | asean.inquiry@sg.tdk.com |
Greater China | Ms. Clover XU | TDK China Co., Ltd. Shanghai, China |
+86 21 61962319 | pr@cn.tdk.com |
Europe | Mr. Frank TRAMPNAU | TDK Management Services GmbH Duesseldorf, Germany |
+49 211 9077 127 | frank.trampnau@managementservices.tdk.com |
America | Ms. Sara M. LAMBETH | TDK Corporation of America Irving, TX, USA |
+1 972-409-4519 | sara.lambeth@us.tdk.com |