Press Release | Oct 30, 2026

TDK showcases sensor and passive component solutions for humanoid robotics at Hon Hai (Foxconn) Tech Day

TDK Corporation (TSE:6762) showcases its diverse portfolio of sensor and passive component solutions for humanoid robotics at Hon Hai (Foxconn) Technology Day, held in Taipei from October 30 to 31, 2026. This portfolio includes position sensing solutions, angle sensors, NTC temperature sensors, and one-stop passive component solutions, demonstrating how TDK supports humanoid robot development across perception, computing, driving, communication, battery management, and human-machine interaction.

With continuous advancements in artificial intelligence, advanced materials, precision motion control, and battery technology, humanoid robots are gradually moving from laboratory displays to industrial applications, demonstrating potential in intelligent manufacturing, logistics, inspection, medical care, and service fields.

Future humanoid robots will not only need to be able to walk, but also achieve precise grasping, dynamic balance, environmental perception, and human-machine collaboration. This places higher demands on electronic components and sensors: the system needs to have high-precision motion sensing, efficient power management, stable high-speed communication, as well as reliability to cope with vibration, temperature changes, and long-term operation.

With its technological expertise in sensors, magnetic components, capacitors, thermistors, power modules, batteries, and EMI noise suppression products, TDK is collaborating with customers to build humanoid robot solutions that cover modules such as sensing, computing, power supply, communication, drive, and dexterous hands, accelerating the transition of innovative achievements from R&D verification to practical application.

High-performance motion and position sensors enable precise control

Sensor solutions for humanoid robots include IMUs, angle sensors, encoders, and position sensors to monitor posture, acceleration, angular velocity, joint position, and actuator status in real time, thereby achieving dynamic balance, precise movements, and safe control.

TDK's MEMS IMU can be considered the "inner ear" of humanoid robots, suitable for the head, torso, hips, feet, and joints. This solution uses low-noise, high-performance gyroscopes and accelerometers, combined with BalancedGyro® vibration suppression technology, effectively reducing the effects of motor noise and structural vibration. The related products support angular velocities up to 4000 dps and acceleration measurement ranges of ±32 g, with support for excellent temperature stability.

In humanoid robot joints, accurate sensing of motor rotor and actuator angular positions plays an important role in improving motion accuracy, operating efficiency, and system safety. TDK TMR angle sensors use the tunnel magnetoresistance (TMR) effect to sense magnetic-field direction, enabling non-contact measurement of angular position. With compact packaging, low power consumption, high sensitivity, and high angular accuracy, these sensors are well suited for space-constrained humanoid robot joint modules, motors, and actuator applications.

In addition, TDK PositionSense™ magnetic position sensing solution by InvenSense, a TDK group company, can detect changes in the magnetic field, enabling non-contact detection of rotational, linear, and switch positions. PositionSense combines a 6-axis IMU and 3-axis TMR-based magnetometer with on-chip sensor fusion software, all in a compact size, simple structure, and with low power consumption and high reliability.

By combining TMR angle sensors, absolute encoders, and related magnetic sensing technologies, TDK can provide diverse position detection solutions for robot joints, motor rotors, linear actuators, and dexterous hands.

Temperature sensing ensures the safety of motors and batteries

Humanoid robots contain numerous motors, actuators, power modules, and battery systems, generating heat during operation. TDK offers glass-encapsulated NTC products, bondable NTC chips, ring-shaped terminal temperature sensors, and high-voltage applications, which can monitor motor windings, drive boards, power devices, computing units, and battery temperatures, helping the system achieve overheat protection.

A highly reliable component solution for actuator communication, haptic feedback, and ESD protection

In order for the humanoid robot industry to make great strides toward the future, high reliability that allows humans to use them with peace of mind will become even more important. TDK’s electronic components are highly reliable parts manufactured with development technology and quality control cultivated over many years in the fields of automotive electronic control units (ECUs) and industrial robots.

For wired communication applications, which serve as the nerves to control actuator motors—key components of humanoid robots—TDK offers products such as CMC (Common Mode Choke), PUI (Power Inductor), and MLCC (Multilayer Ceramic Capacitor), which are widely used in automotive control units and the space industry. TDK develops these products with the aim of further miniaturization, weight reduction, and increased robustness for humanoid robot applications. For better interaction between humans and machines, TDK’s haptics devices enable tactile feedback, and various ESD protection devices make it possible to design systems that do not malfunction due to noise at points of contact with people.

With a product portfolio covering motion sensing, position detection, temperature monitoring, power supply, communications, drive, and tactile feedback, TDK can provide humanoid robot customers with solutions for complete machine systems.

Contacts for regional media

K. Xu

Greater China
TDK (Shanghai) Electronics Ltd.
Shanghai, China
+86 21 2219 1598
Kathy.Xu@tdk.com

About TDK Corporation

TDK Corporation (TSE:6762) is a global technology company and innovation leader in the electronics industry, based in Tokyo, Japan. With the tagline “In Everything, Better” TDK aims to realize a better future across all aspects of life, industry, and society. For over 90 years, TDK has shaped the world from within; from the pioneering ferrite cores to cassette tapes that defined an era, to powering the digital age with advanced components, sensors, and batteries, leading the way towards a more sustainable future. United by TDK Venture Spirit, a start-up mentality built on visions, courage and mutual trust, TDK’s passionate team members around the globe pursue better—for ourselves, customers, partners, and the world. Today, the state-of-the-art technologies of TDK are in everything, from industrial applications, energy systems, electric vehicles, to smartphones and gaming, at the core of modern life. TDK’s comprehensive, innovative-driven portfolio includes cutting-edge passive components, sensors and sensor systems, power supplies, lithium-ion and solid-state batteries, magnetic heads, AI and enterprise software solutions, and more—featuring numerous market-leading products. These are marketed under the product brands TDK, InvenSense, Micronas, Tronics, TDK-Lambda, TDK SensEI, and ATL. Positioning the AI ecosystem as a key strategic area, TDK leverages its global network across the automotive, information and communication technology, and industrial equipment sectors to expand its business in a wide range of fields. In fiscal 2026, TDK posted total sales of USD 16.6 billion and employed about 107,000 people worldwide.