Multilayer Ceramic Capacitors: TDK launches industry-leading low-resistance soft-termination C0G MLCCs with 22 nF at 1000 V in the 3225 case size
- New 1000 V product with a capacitance of 22 nF in the 3225 case size with C0G characteristics of low-resistance soft termination type for automotive and general applications
- Contributes to greater reliability in applications, reduction of component count, and miniaturization
- Qualified based on AEC-Q200
TDK logo is not stamped on the actual product.
September 18, 2025
TDK Corporation (TSE:6762) announced today it expanded its CN series of low-resistance soft-termination MLCCs. This product achieves an industry-leading* 22 nF capacitance in the 3225 case size (3.2 x 2.5 x 2.5 mm – L x W x T) and C0G characteristics at 1000 V. Mass production of the product series began in September 2025. The capacitors of the CN series are industry-first products that are equivalent to regular products in terms of their terminal resistance due to the optimization of their resin electrode structure.
In recent years, there has been an increase in the use of multiple resonance capacitors placed in series-parallel circuits for resonance applications such as LLC resonant circuits and wireless charging. As applications become more powerful, they require more resonance capacitance, which increases the demand for high-voltage, large-volume capacitors. To improve reliability in these applications, components with resin electrodes effectively prevent placement cracks resulting from external stress. However, the increased resistance value of resin electrodes has been an issue.
This led TDK to develop the CN series with optimized resin electrode structures, resulting in significantly lower resistance values. In addition to the low losses and capacitance stability over temperature and voltage variations of C0G products, these resin electrode structures achieve both high reliability against external stress and reduced loss, making them ideal for use as resonator and snubber capacitors.
The optimization of product and process designs has made it possible to manufacture these products, which helps increase reliability and application to high-voltage circuits and enhances the reliability of the applications. TDK will continue to expand its product line to meet the needs of its customers.
* As of September 2025, according to TDK
Main applications
- Resonance circuits
- Snubber circuits
Main features and benefits
- TDK's unique terminal structure realizes soft termination MLCC whose low resistance is equal to that of standard terminal products
- C0G characteristics with low loss and capacitance stability during temperature or voltage changes
- Higher reliability of applications, reduced component count, and miniaturization achieved with resin electrodes, high voltages, and large volume
| Type* | Outer dimensions [mm] |
Temperature characteristics | Rated voltage [V] |
Capacitance [nF] |
Capacitance tolerance [%] |
|---|---|---|---|---|---|
| CNA6P1C0G3A223G250AE | 3.2 x 2.5 x 2.5 | C0G | 1,000 | 22 | ±2 |
| CNA6P1C0G3A223J250AE | ±5 | ||||
| CNC6P1C0G3A223G250AE | ±2 | ||||
| CNC6P1C0G3A223J250AE | ±5 |
*CNA is for automotive, and CNC is for commercial.
Samples may be purchased from the product page displayed after clicking Type.
About TDK Corporation
TDK Corporation (TSE:6762) is a global technology company and innovation leader in the electronics industry, based in Tokyo, Japan. With the tagline “In Everything, Better” TDK aims to realize a better future across all aspects of life, industry, and society. For over 90 years, TDK has shaped the world from within; from the pioneering ferrite cores to cassette tapes that defined an era, to powering the digital age with advanced components, sensors, and batteries, leading the way towards a more sustainable future. United by TDK Venture Spirit, a start-up mentality built on visions, courage and mutual trust, TDK’s passionate team members around the globe pursue better—for ourselves, customers, partners, and the world. Today, the state-of-the-art technologies of TDK are in everything, from industrial applications, energy systems, electric vehicles, to smartphones and gaming, at the core of modern life. TDK’s comprehensive, innovative-driven portfolio includes cutting-edge passive components, sensors and sensor systems, power supplies, lithium-ion and solid-state batteries, magnetic heads, AI and enterprise software solutions, and more—featuring numerous market-leading products. These are marketed under the product brands TDK, EPCOS, InvenSense, Micronas, Tronics, TDK-Lambda, TDK SensEI, and ATL. Positioning the AI ecosystem as a key strategic area, TDK leverages its global network across the automotive, information and communication technology, and industrial equipment sectors to expand its business in a wide range of fields. In fiscal 2025, TDK posted total sales of USD 14.4 billion and employed about 105,000 people worldwide.
Downloads
- Product with background (jpg: 182 KB; 96dpi)
- Product without background (jpg: 120 KB; 96dpi)
- Press release (pdf: 318 KB)
- Further information on the products can be found under
https://product.tdk.com/en/search/capacitor/ceramic/mlcc/list#part_no=CN*C0G3A&_l=50&_p=1&_c=pure_status-pure_status&_d=0
Contacts for regional media
| Region | Contact | Phone | ||
|---|---|---|---|---|
| Japan | Mr. Kotaro Ose | TDK Corporation Tokyo, Japan |
+813 6778-1055 | TDK.PR@tdk.com |
| ASEAN | Ms. Jiang MAN Ms. Pei Lu LEE |
TDK Singapore (Pte) Ltd. Singapore |
+65 6273 5022 | tdk.asean-inquiry@tdk.com |
| Greater China | Ms. Clover XU | TDK China Co., Ltd. Shanghai, China |
+86 21 61962307 | TDK.PR-CN@tdk.com |
| Europe | Mr. Frank TRAMPNAU | TDK Management Services GmbH Duesseldorf, Germany |
+49 211 9077 127 | frank.trampnau@tdk.com |
| America | Ms. Sara M. LAMBETH | TDK Corporation of America Plano, TX, USA |
+1 972-409-4519 | sara.lambeth@tdk.com |