Exhibitions: Experience the future of power solutions with TDK at APEC 2025
- Technologies range within the power electronics industry, including innovations for variable frequency drives, infrastructure power, automotive applications, and more
- TDK is represented from March 17 to 19 in Atlanta, Georgia, at booth 1413
March 10, 2025
TDK Corporation (TSE 6762) will showcase its latest technological developments at APEC 2025, taking place from March 17 to 19 in Atlanta, Georgia. Attendees will have the opportunity to explore TDK’s broad range of power solutions at booth 1413, where experts from product marketing, R&D, and sales will be available to discuss recent innovations.
Technology highlights include:
Industrial & Energy: Reliable power solutions for applications in power protection, conversion, and management.
- Wind Power Generation
Varistors for input/output protection, capacitors for power units (such as the ModCap modular capacitor), and inductors, capacitors, and DC-DC converters for drivers and controllers. - Photovoltaic/Energy Storage Systems
High-voltage capacitors, surge arresters, and thermistors. Additionally offering power capacitors and ferrite cores for booster and DC link applications. - Variable Frequency Drive
Varistors and arresters for input protection, along with power line filters, power line chokes, and LeaXield for both input and output filtering. - EV Fast Charging
Solutions include metalized polypropylene capacitors, and more.
Information & Communication Technologies: Comprehensive power and protection solutions for PoE and LAN systems in infrastructure applications such as servers, base stations, routers, and security cameras.
- Power for Infrastructure
Power and protection building blocks for PoE and LAN applications in servers, base stations, routers, and security cameras. Including common mode filters, high-density power management µPOL, transformers for LAN, surge arrestors, chip varistors, and power inductors.
Automotive: High-performance ADAS and xEV systems for automotive applications with components for telematics, battery management, onboard chargers, and more.
- ADAS
Solutions for telematics, zone controllers, central servers, and more. Featured products include inductors, ceramic chip capacitors, µPOL, chip-embedded DC-to-DC power modules (POL), wireless power transfer solutions, and more. - xEV
Featuring components such as disk varistors, power and film capacitors, thermistors, chip beads, and common mode chokes. Solutions for onboard chargers, battery management systems, DC link applications, and more.
Power Solutions: Advanced AC-DC power supplies and DC-DC converters for innovative industrial, medical, and embedded applications.
- HWS3000G / GT
New compact 3000W industrial programmable power supplies offer Constant Voltage (CV) and Constant Current (CC) operation with single or three-phase inputs. - DUSH960-1248
The new DC-UPS designed for DIN rail mount applications, features a wide programmable input and output voltage range and supports external battery capacities of up to 1000Ah. - CUS800M / CUS1000M
The latest industrial and medical AC-DC power supplies deliver 800W and 1000W in a compact, high-density form factor, featuring a low audible noise variable speed cooling fan. - i1C DC-DC Converter
This new 200W 1”x1” Industry-standard footprint DC-DC converter is the latest addition to our expanding line of industrial non-isolated power module solutions. These buck and buck-boost converters come with various features to meet diverse application needs and help accelerate customers’ time to market.
Programmable Power Supplies: Reliable, high-efficiency solutions for various industrial, test, and measurement applications.
- GenesysTM DC
General-purpose bench-top/rack-mount GenesysTM Programmable DC Power Supplies (750W-15kW) provide the ideal choice for reliable accurate and easy-to-use programmable DC power for everyday technology applications. - GENESYS+TM DC
These Programmable DC Power Supplies (1kW – 22.5kW) and Rack DC Power Systems (30kW-90kW) showcase advanced features, high efficiency, and high power factor for leading-edge high-technology Test & Measurement applications. - GenesysTM AC
The new GenesysTM Programmable AC Power Sources (AC and AC+DC) offers high performance and versatility with 2kVA (or 3kVA) in 1U height and 6kVA (or 9kVA) in three-phase 3U formats.
TDK Seminars: Discussions on power management telemetry for system reliability, the use of xEVCap in EV powertrains, and vertical power delivery, presented by Tony Ochoa, David Olalla, and Bill Pelletier, respectively.
- Industry Session: Ideas for Practical Use Case of Advanced Power Management Telemetry for System Reliability and Predictive Maintenance
Presenter: Tony Ochoa, TDK Marketing Director - POL Power Group
Date: Tuesday, March 18, 2025 @ 9:20 AM ET
Location: Level Four, A404/A405 - Dialogue Session: A Practical Use of xEVCap: The Modular and Standard DC-Link Capacitor Solution for the Main EV Powertrain Inverter
Presenter: David Olalla, TDK Electronics Vice President - Product Development Film Capacitors Industry & Automotive
Date: Thursday, March 20, 2025 @ 11:30 AM
Location: Level One, Hall A3 - Exhibitor Presentation: Stacking the Deck for Vertical Power Delivery
Presenter: Bill Pelletier, TDK Faraday Semi, Inc. Field Application EngineerDate: Wednesday, March 19, 2025 @ 12:00 PMLocation: Expo Theater 4
About TDK Corporation
TDK Corporation is a world leader in electronic solutions for the smart society based in Tokyo, Japan. Built on a foundation of material sciences mastery, TDK welcomes societal transformation by resolutely remaining at the forefront of technological evolution and deliberately “Attracting Tomorrow.” It was established in 1935 to commercialize ferrite, a key material in electronic and magnetic products. TDK‘s comprehensive, innovation-driven portfolio features passive components such as ceramic, aluminum electrolytic and film capacitors, as well as magnetics, high-frequency, and piezo and protection devices. The product spectrum also includes sensors and sensor systems such as temperature and pressure, magnetic, and MEMS sensors. In addition, TDK provides power supplies and energy devices, magnetic heads and more. These products are marketed under the product brands TDK, EPCOS, InvenSense, Micronas, Tronics and TDK-Lambda. TDK focuses on demanding markets in automotive, industrial and consumer electronics, and information and communication technology. The company has a network of design and manufacturing locations and sales offices in Asia, Europe, and in North and South America. In fiscal 2024, TDK posted total sales of USD 14.6 billion and employed about 101,000 people worldwide.
Contacts for regional media
| Region | Contact | Phone | ||
|---|---|---|---|---|
| Global | Ms. Sara LAMBETH | TDK Corporation of America Plano, TX, USA |
+1 972-409-4519 | Sara.Lambeth@tdk.com |
| North America | Ms. Sarah MACKENZIE | Publitek Portland, OR |
+1 503-720-3743 | TDK-global@publitek.com |