News Center | Press Releases

Radio wave absorbers: TDK launches environmentally sustainable radio wave absorbers using biomass material

  • Officially approved by the Japan BioPlastics Association (JBPA)
  • By including more than 25 wt% of biomass material, it enables a reduction of CO₂ emissions by 13% compared to conventional products
press_01_240530_01.jpg
Registration No. 1191,1192

May 30, 2024

TDK Corporation (TSE:6762) announces its new radio wave absorber IS-BP series, containing more than 25 wt% of biomass material, making it an environmentally sustainable option that enables CO₂ reduction. Mass production started in April 2024.

Microwave anechoic chambers are used to evaluate antennas and wireless communication equipment, as well as millimeter-wave radar for AD and ADAS. The ceiling, walls, and floor of the microwave anechoic chamber are covered with radio wave absorbers.

press_01_240530_03

TDK’s radio wave absorber IS-BP series is made of foamed polyethylene with carbon dispersed in it; it absorbs radio waves by utilizing ohmic loss of the carbon. The shape is pyramidal with lengths available 12 cm and 30 cm depending on the frequency range used.

The absorption performance of the IS-BP series is equivalent to that of conventional products. Additionally, extensive testing has shown that the IS-BP series is as strong and durable as traditional products and is equally non-flammable.

The new IS-BP series contains over 25 wt% of biomass polyethylene derived from sugarcane, replacing petroleum-derived polyethylene. TDK is committed to maximizing its contribution to the creation of a sustainable society by working alongside its customers in a wide range of applications, including automotive, ICT, and industrial equipment. The new absorber material was developed in response to the growing demand of supply chain partners to show compliance with climate change initiatives. This new sustainable product is certified by the JBPA and has been shown to reduce CO₂ emissions by 13% compared to conventional products.

Main applications

  • Microwave and EMC anechoic chambers for evaluation of antennas and wireless communication devices, and evaluation of mmWave radar for AD/ADAS, EMC measurement above GHz band

Main features and benefits

  • Environmentally sustainable radio wave absorber using biomass material
  • Approved by the JBPA
  • Contains more than 25 wt% of biomass material
  • CO₂ emissions can be reduced by 13% compared to conventional products
  • Equivalent performance and flame retardance to conventional products

Key data

Typical absorption performance at certain frequencies (normal incidence); Unit: dB

Product Name 0.8 GHz 1 GHz 3 GHz 5 GHz 10 GHz 30 GHz 50 GHz 110 GHz
IS-012A-BP 20 20 30 40 55 55 55 50
IS-030A2-BP 30 35 45 50 55 55 55 50

About TDK Corporation

TDK Corporation is a world leader in electronic solutions for the smart society based in Tokyo, Japan. Built on a foundation of material sciences mastery, TDK welcomes societal transformation by resolutely remaining at the forefront of technological evolution and deliberately “Attracting Tomorrow.” It was established in 1935 to commercialize ferrite, a key material in electronic and magnetic products. TDK‘s comprehensive, innovation-driven portfolio features passive components such as ceramic, aluminum electrolytic and film capacitors, as well as magnetics, high-frequency, and piezo and protection devices. The product spectrum also includes sensors and sensor systems such as temperature and pressure, magnetic, and MEMS sensors. In addition, TDK provides power supplies and energy devices, magnetic heads and more. These products are marketed under the product brands TDK, EPCOS, InvenSense, Micronas, Tronics and TDK-Lambda. TDK focuses on demanding markets in automotive, industrial and consumer electronics, and information and communication technology. The company has a network of design and manufacturing locations and sales offices in Asia, Europe, and in North and South America. In fiscal 2024, TDK posted total sales of USD 14.6 billion and employed about 101,000 people worldwide.

Downloads

Contacts for regional media

Region Contact Phone Mail
Japan Mr. Yoichi OSUGA TDK Corporation
Tokyo, Japan
+813 6778-1055 TDK.PR@tdk.com
ASEAN Ms. Jiang MAN
Ms. Pei Lu LEE
TDK Singapore (Pte) Ltd.
Singapore
+65 6273 5022 tdk.asean-inquiry@tdk.com
Greater China Ms. Clover XU TDK China Co., Ltd.
Shanghai, China
+86 21 61962307 TDK.PR-CN@tdk.com
Europe Mr. Frank TRAMPNAU TDK Management Services GmbH
Duesseldorf, Germany
+49 211 9077 127 frank.trampnau@tdk.com
America Ms. Sara M. LAMBETH TDK Corporation of America
Plano, TX, USA
+1 972-409-4519 sara.lambeth@tdk.com