EMC Components: TDK expands notch filter lineup with built-in ESD protection function
- New notch filters achieve both ESD protection and noise suppression up to the maximum frequency of 5.3 ㎓ band
- Suppression of TDMA noise generated in wireless communication and increased wireless signal reception sensitivity
- Strong electrostatic protection capability (compliant with IEC61000-4-2 Level 4)
March 15, 2022
TDK Corporation (TSE:6762) announces the release of its newly developed AVRF041A150MT242 and AVRF061D2R4ST532 notch filters with ESD protection function. Volume production of these devices will begin in March 2022.
The new notch filters are compliant with the IEC61000-4-2 Level 4 immunity standard. They are well suited to ensuring EMC requirements are met in the audio circuits of key applications - including smartphones, wireless earbuds (TWS), and smart speakers. Thanks to TDK's proprietary materials and advanced structural design, the new products implement industry-leading attenuation characteristics for specific frequency bands. They are highly effective at noise suppression and improved reception sensitivity in wireless communication. Moreover, the products can simultaneously provide countermeasures against both noise and ESD via one single chip, both reducing costs and using less board real estate.
The AVRF041A150MT242 features a small footprint of only 0.4 x 0.2 x 0.2 ㎜ and delivers ESD protection and noise suppression in the 2.4 ㎓ band. It has a maximum insertion loss of just -20㏈ at 2.4㎓, The AVRF061D2R4ST532, which is supplied in 0.6 x 0.3 x 0.3 ㎜ form factor offers ESD protection and noise suppression in the frequency band up to 5.3㎓. At that frequency, it has a -15㏈ insertion loss.
With accelerating 5G transition and advanced mutual coordination between connected equipment, the era of IoT is now here. In addition to the conventional demands for lower power consumption and increased functionality, electronic equipment is required to have higher quality design and exhibit ongoing operational reliability. By developing notch filter solutions with significantly smaller footprints and expanded frequency capabilities, TDK is able to address market expectations for more streamlined telecommunication devices, such as smartphones and TWS, while also expanding the frequency band in relation to the latest generation of Wi-Fi transmissions.
Moving forward, TDK will continue to expand its product lineup to meet the needs for diversified telecom applications.
Glossary
- EMC: Electromagnetic compatibility
- ESD: Electrostatic discharge
- TDMA noise: Unpleasant audible noise generated by speakers when high frequency communication signals intrude into a microphone line
- IEC61000-4-2: An immunity standard for electrostatic discharge established by ( the International Electrotechnical Commission (IEC)
Main applications
- Protection against noise and ESD for audio equipment using Wi-Fi, Bluetooth and other wireless forms of communication in the frequency band between 1.0 ㎓ and 5.3 ㎓
Main features and benefits
- Providing measures for both ESD protection and noise
- Compliant with IEC61000-4-2 Level 4
- The smallest footprint in the lineup (0402 size format)
Key data
| Type | Outer dimensions [㎜] |
Maximum allowable circuit voltage [V] |
Capacitance [㎊] |
Insertion loss [㏈] |
|---|---|---|---|---|
| AVRF041A150MT242 | 0.4 x 0.2 x 0.2 (EIA01005) |
10 max. | 15 ㎊ ± 20 % | -20 max.at 2.4 ㎓ |
| AVRF061D2R4ST532 | 0.6 x 0.3 x 0.3 (EIA0201) |
20 max. | 2.4 ㎊ ± 0.4 ㎊ | -15 max.at 5.3 ㎓ |
Complete product portfolio of notch filters with built-in ESD protection function
| Band of noise suppression | Audio Recommended circuit |
0.4 x 0.2 x 0.2 ㎜[EIA01005] | 0.6 x 0.3 x 0.3 ㎜[EIA0201] | 1.0 x 0.5 x 0.5 ㎜[EIA0402] | 1.6 x 0.8 x 0.8 ㎜[EIA0603] |
|---|---|---|---|---|---|
| Measures for Wi-Fi band (5 ㎓) |
Headphone/ Microphone/ speaker/ receiver |
AVRF061D2R4ST532 20V, 5.3 ㎓ |
|||
| Measures for Bluetooth & Wi-Fi band (2.4 ㎓) |
Headphone/ microphone |
AVRF041A150MT242 10 V, 2.4 ㎓ |
AVRF060X100LT242 7 V, 2.4 ㎓ |
AVRF101U6R8KT242 28 V, 2.4 ㎓ |
|
| Speaker/ receiver |
AVRF061P160MT212 12 V, 2.1 ㎓ |
||||
| Measure for cellular band (700 M -2.7 ㎓) |
Microphone | AVRF060V600MT102 3.5 V, 1.0 ㎓ |
|||
| Headphone | AVRF060W650MT102 5.5 V, 1.0 ㎓ |
||||
| Speaker/ receiver |
AVRF061P160MT212 12 V, 2.1 ㎓ |
||||
| Measure for Class D amplifier noise (100 M -400 ㎒) |
Speaker/ receiver |
AVRF161Q861LT201 19 V, 200 ㎒ |
About TDK Corporation
TDK Corporation is a world leader in electronic solutions for the smart society based in Tokyo, Japan. Built on a foundation of material sciences mastery, TDK welcomes societal transformation by resolutely remaining at the forefront of technological evolution and deliberately “Attracting Tomorrow.” It was established in 1935 to commercialize ferrite, a key material in electronic and magnetic products. TDK's comprehensive, innovation-driven portfolio features passive components such as ceramic, aluminum electrolytic and film capacitors, as well as magnetics, high-frequency, and piezo and protection devices. The product spectrum also includes sensors and sensor systems such as temperature and pressure, magnetic, and MEMS sensors. In addition, TDK provides power supplies and energy devices, magnetic heads and more. These products are marketed under the product brands TDK, EPCOS, InvenSense, Micronas, Tronics and TDK-Lambda. TDK focuses on demanding markets in automotive, industrial and consumer electronics, and information and communication technology. The company has a network of design and manufacturing locations and sales offices in Asia, Europe, and in North and South America. In fiscal 2021, TDK posted total sales of USD 13.3 billion and employed about 129,000 people worldwide.
Downloads
- Further information on the products can be found under
https://product.tdk.com/system/files/dam/doc/product/emc/emc/esd-notch/catalog/notch-filter_commercial_avrf_en.pdf
Contacts for regional media
| Region | Contact | Phone | ||
|---|---|---|---|---|
| Japan | Mr. Yoichi OSUGA | TDK Corporation Tokyo, Japan |
+813 6778-1055 | pr@jp.tdk.com |
| ASEAN | Ms. Jiang MAN Ms. Pei Lu LEE |
TDK Singapore (Pte) Ltd. Singapore |
+65 6273 5022 | asean.inquiry@sg.tdk.com |
| Greater China | Ms. Clover XU | TDK China Co., Ltd. Shanghai, China |
+86 21 61962307 | pr@cn.tdk.com |
| Europe | Mr. Frank TRAMPNAU | TDK Management Services GmbH Duesseldorf, Germany |
+49 211 9077 127 | frank.trampnau@tdk.com |
| America | Ms. Sara M. LAMBETH | TDK Corporation of America Irving, TX, USA |
+1 972-409-4519 | sara.lambeth@us.tdk.com |