News Center | Press Release
(Revision) Partial Revision to “Announcement on Business Alliance and Establishment of Joint Venture with Contemporary Amperex Technology Co., Limited”
May 13, 2021
TDK Corporation (the “Company”) hereby announces that there were misstatements in a part of the “Announcement on Business Alliance and Establishment of Joint Venture with Contemporary Amperex Technology Co., Limited” announced on April 28, 2021, and revisions are made as outlined below. The revised parts are underlined.
1. Reason of revision
The Company makes a revision because there was an error in the description of the equity ratio in Amperex Technology Limited, a consolidated subsidiary of the Company.
2. Details of revision
【Before revision】
3. Overview of the consolidated subsidiaries of the Company
| (10) | Equity ratio | 99.7% (as of 2021/03/31) |
【After revisionn】
3. Overview of the consolidated subsidiaries of the Company
| (10) | Equity ratio | 100% (as of 2021/03/31) |
Contacts for media
| Contact | Phone | ||
|---|---|---|---|
| Mr. Kazushige Atsumi | TDK Corporation | +81 3 6778-1055 | TDK.PR@tdk.com |