Magnetic sensors: Joint development of high accuracy TMR 3-axis magnetometer with Asahi Kasei Microdevices
- Combines TDK’s high accuracy TMR element with Asahi Kasei Microdevices’ advanced electronic compass ASIC
- High sensitivity of 10 nT/LSB
- Industry’s lowest RMS noise of just 40 nT-rms
January 9, 2018
TDK Corporation and Asahi Kasei Microdevices Corporation (AKM) have jointly developed a highly accurate 3-axis magnetometer that combines an extremely sensitive tunnel magneto-resistive (TMR) element developed by TDK and an advanced electronic compass ASIC designed by AKM in a very small package. The new TMR magnetometer on a chip, which has miniature dimensions of just 1.6 mm x 1.6 mm x 0.6 mm, features the industry’s lowest RMS noise of just 40 nT-rms and a very low current consumption of only 40 µA at an output data rate of 100 Hz.
Thanks to its high sensitivity of 10 nT/LSB*, the magnetic sensor can detect minute changes in magnetic fields very precisely, enabling the highly accurate detection of both position and orientation with the help of the Earth’s magnetic field or a magnetic field generator. These unique characteristics make the TMR magnetometer ideal for compact electronic devices such as smartphones, tablets, game console controllers and all kinds of wearable devices, as well as other applications that demand high position and orientation precision such as virtual, augmented or mixed reality (VR, AR, and MR) or indoor navigation. The new 3-axis magnetic sensor is also suitable for integration into IoT devices, for which strong market growth is expected.
The new sensor will be on display at the booths of both TDK and AKM at the Consumer Electronics Show 2018 (CES 2018), the world’s largest electronics exhibition, which will take place in Las Vegas, USA, from January 9 to 12, 2018.
* Least Significant Bit
Glossary
-
- TMR: Tunnel magneto resistance. Of all magnetic field sensors, this offers the greatest sensitivity
Main applications
-
- Compact electronic devices such as smartphones, tablets and game console controllers
- All kinds of wearable devices or IoT devices
- Applications that demand high position and orientation precision such as virtual, augmented or mixed reality (VR, AR, and MR) or indoor navigation
Main features and benefits
-
- High sensitivity of 10 nT/LSB
- Industry’s lowest RMS noise of just 40 nT-rms
- Very low current consumption of only 40 µA at an output data rate of 100 Hz
- Miniature dimensions of just 1.6 mm x 1.6 mm x 0.6 mm
Key data
| Measurement range | [μT] | ±1200 |
|---|---|---|
| Sensitivity | [nT/LSB] | 10 |
| RMS noise (typ.) | [nT-rms] | 40 |
| Output bit | [bits] | 18 |
| Current consumption @ ODR of 100 Hz | [μA] | 40 |
| Dimensions | [mm] | 1.6 x 1.6 x 0.6 |
New product introduction
| Exhibition | Consumer Electronics Show 2018 (CES 2018) |
|---|---|
| Venue | Las Vegas Convention & World Trade Center (LVCC) |
| Dates | January 9 to 12, 2018 |
| Location | AKM:Venetian Suites 30-209, 30-211; Invitation only To request an appointment please visit: www.akmsj.com |
About Asahi Kasei Microdevices Corporation
Asahi Kasei Microdevices Corporation (AKM*), a group company of Asahi Kasei Corporation, is a Japan-based company which has continued to provide customers with optimum solutions all over the world for over 30 years by offering a variety of advanced sensing devices based on compound semiconductor technology and sophisticated IC products featuring analog/digital mixed-signal technology.
* AKM is a trademark of Asahi Kasei Microdevices Corporation in Japan, Europe and the United States.
About TDK Corporation
TDK Corporation is a leading electronics company based in Tokyo, Japan. It was established in 1935 to commercialize ferrite, a key material in electronic and magnetic products. TDK's portfolio includes passive components, such as ceramic, aluminum electrolytic and film capacitors, ferrites and inductors, high-frequency products, and piezo and protection components, as well as sensors and sensor systems and power supplies. These products are marketed under the product brands TDK, EPCOS, InvenSense, Micronas, Tronics and TDK-Lambda. TDK's further main product groups include magnetic application products, energy devices, and flash memory application devices. TDK focuses on demanding markets in the areas of information and communication technology and automotive, industrial and consumer electronics. The company has a network of design and manufacturing locations and sales offices in Asia, Europe, and in North and South America. In fiscal 2017, TDK posted total sales of USD 10.5 billion and employed about 100,000 people worldwide.
Downloads
Contacts for regional media
| Region | Contact | Phone | ||
|---|---|---|---|---|
| Japan | Mr. Yoichi OSUGA | TDK Corporation Tokyo, Japan |
+813 6852-7102 | TDK.PR@tdk.com |
| ASEAN | Ms. Jiang MAN Ms. Pei Lu LEE |
TDK Singapore (Pte) Ltd. Singapore |
+65 6273 5022 | TDK.ASEAN-inquiry@tdk.com |
| Greater China | Ms. Clover XU | TDK China Co., Ltd. Shanghai, China |
+86 21 61962319 | TDK.PR-CN@tdk.com |
| Europe | Mr. Frank TRAMPNAU | TDK Europe GmbH Duesseldorf, Germany |
+49 211 9077 127 | frank.trampnau@eu.tdk.com |
| America | Ms. Sara M. LAMBETH | TDK Corporation of America Irving, TX, USA |
+1 972-409-4519 | sara.lambeth@tdk.com |