EMC Components:High-impedance chip beads with lowest DC resistance
- Lowest DC resistance for a chip bead of its size
 - 20 percent higher impedance than existing chip beads with the same DC resistance
 - Compact dimensions of 0.4 mm x 0.2 mm x 0.2 mm
 

Aug. 29, 2017
TDK Corporation announced the development of the MMZ0402EUC series of chip beads, with the lowest DC resistance for a chip bead its size*. The two new types with their respective impedance values of 150 Ω and 180 Ω at 100 MHz, feature DC resistance values of only 0.62 Ω and 0.69 Ω. This results in a significant reduction in power losses, while at the same time providing excellent noise suppression. In fact, the compact IEC 0402 components with dimensions of 0.4 mm x 0.2 mm x 0.2 mm feature an impedance that is up to 20 percent higher than TDK's existing MMZ chip beads with the same DC resistance rating. Combined with their higher rated currents of 350 mA and 300 mA compared to existing types, the new MMZ0402EUC chip beads are ideally suited for noise suppression in the power and signal circuits of smartphones, tablets and other mobile devices. Mass production was launched in August 2017.
The improved ratio of impedance to DC resistance of the new series was achieved thanks to advanced TDK materials. The components can be used in a wide range of temperatures from -55 °C to +125 °C. TDK will continue to expand the available range of impedance values in the compact lineup to meet the requirements for a broad range of mobile device designs.
* As of August 2017, according to TDK research
Main applications
- 
- Smartphones, tablets, and other mobile devices
 
 
Main features and benefits
- 
- Lowest DC resistance for a chip bead of its size, with values as low as 0.62 Ω
 - Impedance of 150 Ω and 180 Ω at 100 MHz is up to 20 percent higher than that of existing chip beads with the same DC resistance
 - Compact dimensions of just 0.4 mm x 0.2 mm x 0.2 mm
 - Wide operating temperature range from -55 °C to +125 °C
 
 
Key data
- 
Type Dimensions 
[mm]Impedance 
[Ω] at 100 MHz typ.*Impedance 
[Ω] at 700 MHz typ.*DC resistance 
[Ω] max.Rated current 
[mA] max.MMZ0402EUC151C 0.4 x 0.2 x 0.2 150 340 0.62 350 MMZ0402EUC181C 180 400 0.69 300 * Tolerance ±25%
 
About TDK Corporation
TDK Corporation is a leading electronics company based in Tokyo, Japan. It was established in 1935 to commercialize ferrite, a key material in electronic and magnetic products. TDK's portfolio includes passive components, such as ceramic, aluminum electrolytic and film capacitors, ferrites and inductors, high-frequency products, and piezo and protection components, as well as sensors and sensor systems and power supplies. These products are marketed under the product brands TDK, EPCOS, InvenSense, Micronas, Tronics and TDK-Lambda. TDK's further main product groups include magnetic application products, energy devices, and flash memory application devices. TDK focuses on demanding markets in the areas of information and communication technology and automotive, industrial and consumer electronics. The company has a network of design and manufacturing locations and sales offices in Asia, Europe, and in North and South America. In fiscal 2017, TDK posted total sales of USD 10.5 billion and employed about 100,000 people worldwide.
Downloads
- Further information on the products can be found under https://product.tdk.com/info/en/catalog/datasheets/beads_commercial_signal_mmz0402_en.pdf .
 
Contacts for regional media
| Region | Contact | Phone | ||
|---|---|---|---|---|
| Japan | Mr. Yoichi OSUGA | TDK Corporation Tokyo, Japan  | 
+81 3 6778-1055 | TDK.PR@tdk.com | 
| ASEAN | Ms. Jiang MAN Ms. Pei Lu LEE  | 
TDK Singapore (Pte) Ltd.Singapore | +65 6273 5022 | TDK.ASEAN-inquiry@tdk.com | 
| Greater China | Ms. Clover XU | TDK China Co., Ltd. Shanghai, China  | 
+86 21 61962319 | TDK.PR-CN@tdk.com | 
| Europe | Mr. Frank TRAMPNAU | TDK Europe GmbH Duesseldorf, Germany  | 
+49 211 9077 127 | frank.trampnau@eu.tdk.com | 
| America | Ms. Sara M. LAMBETH | TDK Corporation of America Irving, TX, USA  | 
+1-972-409-4519 | sara.lambeth@tdk.com |