News Center | Press Releases

Power Management Products: TDK announces new ultra-low profile μPOL™ DC-DC converters

  • Advanced ultra-low profile packaging and 3D technology are key drivers for next-generation high performance energy efficient designs
  • High-density solution for space-constrained applications requiring a low-profile power source
  • Scalable and highly configurable with multi-time programmable memory, offering a wide range of flexibility using Digital Communication (I2C and PMBUS)
  • Premiering at APEC 2022 in Houston, TX, March 20-24, TDK booth #814
Power Management Products: TDK announces new ultra-low profile µPOL™ DC-DC converters

March 17, 2022

TDK Corporation (TSE:6762) announces the availability of FS1412 microPOL (μPOL™) power module. At 5.8. ㎜ x 4.9 ㎜ x 1.6 ㎜ (L x W x T), the FS1412 is part of a new series of μPOL™ DC-DC converters with increased performance, smallest available size, ease of use, and simplified integration for applications such as big data, machine learning, artificial intelligence (AI), 5G cells, IoT networking, telecommunication, and computing enterprise. μPOL technology includes a DC-DC converter placed in the vicinity of complex chipsets such as ASICs, FPGAs, and others. By minimizing the distance between the converter and the chipset, the resistance and the inductance components are minimized, allowing fast response and accurate regulation with dynamic load currents. Mass production of FS1412 started in Q4 2021.

TDK has been developing this technology over several years to enable system level solutions to enhance electrical and thermal performance focusing on high-density cost-effective solutions for space-constrained applications which require a low-profile power source. These new solutions incorporate high-performance semiconductors in advanced packaging technologies such as semiconductor embedded in substrate (SESUB) and advanced electronic components to achieve unique system integration in a smaller size and lower profile by 3D integration. This integration allows TDK to deliver higher efficiency and ease of use at a lower total system cost to what is currently available today.

The new µPOL DC-DC converters series operates at a broad junction temperature range, from -40 ℃ to 125 ℃ and features a high current density of more than 1000 A per cubic inch. The series delivers at 12 A with the lowest commercially available height at 1.6 ㎜, while offering 50% less solution size than the other products available in its class. As a result, this minimizes system solution cost, reduces board size and assembly costs, as well as BOM and PCB costs.

TDK will be showcasing its µPOL technology and full line-up of compact power solutions at the APEC 2022 event from March 20-24, George R. Brown Convention Center in Houston, TX, USA at booth #814.

Glossary

  • μPOL and nPOL are integrated DC-DC converters placed in the vicinity of complex ICs such as ASICs, FPGAs, and others

Main applications

  • Network Storage: Enterprise SSD / Storage Area Network
  • Servers: Main Stream Server, Rack and Blade Server, Micro Server
  • Netcoms and Telecoms: Ethernet Switch and Router and 5G Small Cells and 5G Base Stations

Main features and benefits

  • Footprint of 5.8 x 4.9 x 1.6 ㎜ (L x W x T)
  • Output current rated at 12 A, with 50% less required capacitance than existing products
  • Suitable for a junction temperature range from -40 ℃ to 125 ℃
  • Lead free and RoHS/WEEE compliant

Key data

Type Dimensions [㎜] Rated current [A]
FS1412 5.8 x 4.9 x 1.6 12

About TDK Corporation

TDK Corporation is a world leader in electronic solutions for the smart society based in Tokyo, Japan. Built on a foundation of material sciences mastery, TDK welcomes societal transformation by resolutely remaining at the forefront of technological evolution and deliberately “Attracting Tomorrow.” It was established in 1935 to commercialize ferrite, a key material in electronic and magnetic products. TDK's comprehensive, innovation-driven portfolio features passive components such as ceramic, aluminum electrolytic and film capacitors, as well as magnetics, high-frequency, and piezo and protection devices. The product spectrum also includes sensors and sensor systems such as temperature and pressure, magnetic, and MEMS sensors. In addition, TDK provides power supplies and energy devices, magnetic heads and more. These products are marketed under the product brands TDK, EPCOS, InvenSense, Micronas, Tronics and TDK-Lambda. TDK focuses on demanding markets in automotive, industrial and consumer electronics, and information and communication technology. The company has a network of design and manufacturing locations and sales offices in Asia, Europe, and in North and South America. In fiscal 2021, TDK posted total sales of USD 13.3 billion and employed about 129,000 people worldwide.

Downloads

Contacts for regional media

Region Contact Phone Mail
Japan Mr. Yoichi OSUGA TDK Corporation
Tokyo, Japan
+813 6778-1055 TDK.PR@tdk.com
ASEAN Ms. Jiang MAN
Ms. Pei Lu LEE
TDK Singapore (Pte) Ltd.
Singapore
+65 6273 5022 TDK.ASEAN-inquiry@tdk.com
Greater China Ms. Clover XU TDK China Co., Ltd.
Shanghai, China
+86 21 61962319 TDK.PR-CN@tdk.com
Europe Mr. Frank TRAMPNAU TDK Management Services GmbH
Duesseldorf, Germany
+49 211 9077 127 frank.trampnau@.tdk.com
America Mr. David A. ALMOSLINO TDK USA
San Jose, CA
+1 408-501-2278 david.almoslino@tdk.com
America Ms. Sarah MACKENZIE Publitek
Portland, OR
+1 503-720-3743 TDK-US@publitek.com