Exhibitions
Understand in simple terms the close relationship between electricity and magnetism with Faraday’s famous laws of electromagnetic induction. You can experience electromagnetic induction, which is when electricity is generated at both ends of a coil as a magnet is moved close to it.
It was the experimental equipment used for the Einstein–de Haas effect that demonstrated the gyromagnetic effect, which is the basic principle of “spintronics,” now at the cutting edge of magnetics. This is said to be the Einstein’s only published experiment in his lifetime.
You can learn in a simple and hands-on way about the gyromagnetic effect, which is the basic principle of spintronics, with two types of trial kits for the Einstein–de Haas effect and the Barnett effect respectively.
Curated by the leading authority in spintronics,
Prof. Koki Takanashi, Director of the Institute for Materials Research at Tohoku University
-
Technical support: JST ERATO Saitoh Spin Quantum Rectification Project

Experimental demonstration of the Einstein–de Haas effect
Spintronics is a technology at the leading edge of magnetics. It is based on gyromagnetic properties known as the Einstein–de Haas effect. The experimental setup used for proving the effect is illustrated in an easy-to-understand format by this exhibit.
Future Zone