In October 2016, TDK completed a building on the site of its Honjo Factory in Akita Prefecture as a new production site for electronic components and a new building at the site of its Inakura Factory in Nikaho City, Akita Prefecture.
Previously, TDK reinforced its business sites in the Akita region as electronic component production sites for global markets, but going forward, we will establish new strategic production sites in Akita to conduct more intensive and efficient production of electronic components as a part of our growth strategy for achieving success in the highly competitive global market. These production sites will encourage the sharing of core technologies, such as magnetic materials technologies, which are part of TDK's DNA, as well as improvements in processes so that we can increase the speed of customer response even further and quickly launch new businesses and new products in the future.
The new plants are also production sites that achieve “TDK Industry 4.5.” “Industry 4.0” is a movement promoted through collaboration among German industry, government, and academia with the aim of minimizing costs by greatly raising the levels of digitization, automatization, and virtualization of production processes much higher than those of today. TDK added “0.5” to this concept to represent the pursuit of zero defect quality based on advanced technological capabilities to create “TDK Industry 4.5,” an original TDK initiative. In addition, the two new factories in Akita will support the realization of “location free” production, which will enable TDK to achieve uniform quality on a global level.
The new plants are also production sites that achieve “TDK Industry 4.5.” “Industry 4.0” is a movement promoted through collaboration among German industry, government, and academia with the aim of minimizing costs by greatly raising the levels of digitization, automatization, and virtualization of production processes much higher than those of today. TDK added “0.5” to this concept to represent the pursuit of zero defect quality based on advanced technological capabilities to create “TDK Industry 4.5,” an original TDK initiative. In addition, the two new factories in Akita will support the realization of “location free” production, which will enable TDK to achieve uniform quality on a global level.
                        
                        
                        
                    Monitoring system networks made up of cameras and sensors in the factories autonomously detect process problems on the manufacturing line in real time and, if a problem occurs, stop the line to prevent products from being released. The system allows for automatic normalization using feedback from analysis conducted through cloud computing. Innovations are also being implemented in inventory management and energy efficiency.
                        
                        * An image of production equipment
                    The key to achieving zero defect quality is establishing upstream control. The aim is to attain zero defect in all areas, including design, materials, processes, and management. To do this, robots and sensors are used, and feedback derived from data is comprehensively applied. Information collected by sensors is utilized as Big data. The information is extensively analyzed and used for temperature, air pressure, and humidity control to link everything for integrated operation.
The use of robots is also important for conducting manufacturing with minimal operations by personnel. This will make it possible to achieve location free production that can maintain uniform quality regardless of the production site. TDK is not simply pursuing full automation or unmanned production but is building ideal lines in all areas, including lead times, production, and logistics, through the optimal placement of people and robots.
                        
                    The new buildings were designed to raise energy efficiency through such innovations as storing accumulated snow that falls in the winter to support cold recovery. Solar panels installed on the roof of the Honjo Factory East Site can generate up to 70% of the electric power used for lighting the entire site. In addition, the two buildings were designed with an awareness of creating an employee-friendly environment, such as snow-melting equipment in parking areas and on-site arcades, and the buildings are also expected to play a role as next-generation model environment-adapted factories.
                        
                    
                        TDK will create a world-leading factory as a platform for state-of-the-art Monozukuri
Strengthening of Monozukuri was a major topic for TDK. The concept for the new Akita factories has its roots in the structural reform period that began in fiscal 2012. At the time, the competitiveness of our multilayer ceramic capacitors, which were one of our major products, decreased and the business became unprofitable. This was due to the fact that we were trailing competitors in terms of quality, lead time, and production costs, among other factors. Our factories in the Akita area were aging, and the need to move products between factories at scattered locations was hurting efficiency.
There was discussion whether production should be moved overseas, where costs were more competitive. One possibility would have been to avoid China with its rising labor costs and go to Southeast Asia or a similar location, but we realized that this would eventually lead to a dead end. Furthermore, developments such as the increasing use of electronics in automobiles and the onset of the IoT society are creating a world where electronic components are ever more intricately linked with daily life, and their quality therefore is an increasingly important factor. With the intent to create a vibrant place where the latest techniques could flourish and where products that are competitive in many aspects could be manufactured, construction of two new factories was completed in October 2016.
The essential ideas behind the “Industry 4.0” concept promoted by the German government in cooperation with industry and academia are the reduction of personnel requirements and lower costs. Making efforts to keep investments of people and capital as low as possible while increasing production efficiency is an approach that does not differ significantly from the direction in which we are headed. But our new plants are adding “0.5” to the equation by aiming to ensure that no defective product is shipped to the customer, thereby providing added value and resulting in “TDK Industry 4.5.”
The keywords for creating a framework that does not produce defective goods are “Materials” × “Processes” × “Optimization.” In concrete terms, this means that the design already reflects the way the customer's end product will be used, and the material is developed to elevate the quality of the finished product to the ultimate level. Within each process, the conditions for creating a conforming product are clarified and thorough process step design reflecting the methods and intended outcome is harnessed for strengthened quality management. This will enable the realization of zero defect quality.
Reduction of lead time is also a major factor in creating value for customers. To name one example, the Direct Sintering System (DSS) used in our ferrite production lines results in shorter pressing and firing processes. Stated in simple terms, the ideal is to “insert powder and get a finished coil.” We are also increasingly using robots, and we are not limiting ourselves to single-purpose types. Rather, we aim to utilize versatile robots that can perform multiple functions. Combining these efficiently with human labor is the key for increased productivity. By configuring integrated material + product lines, we will be creating a Monozukuri paradigm that results in consistent product output that is completely independent of the production location.
View the full text of “TDK's Future Strategy” on the PDF version.
TDK's Future Strategy