News Center | Press Releases

Actuators with haptic feedback: Ultra-thin PiezoHapt actuator with low driving voltage

Actuators with haptic feedback  Ultra-thin PiezoHapt™ actuator with low driving voltage

Feb. 14, 2017

TDK has expanded its portfolio of haptic components with the new ultra-thin PiezoHapt actuator featuring a very short response time of just 4 ms. PiezoHapt has a unimorph design consisting of a multilayer piezo element bonded to one side of a vibration plate. With a thickness of a mere 0.35 mm the new haptic actuator is much thinner than conventional eccentric rotary motors and linear resonant actuators, and one of the world's thinnest haptic devices. Moreover, thanks to its fast rise time, PiezoHapt represents a power-saving solution compared to conventional solutions. Shipments of samples will begin in March 2017.

The actuator can be driven with low voltages of ≤24 V and can produce a wide variety of vibration patterns, depending on the amplitude and frequency of the voltage applied. The new PHUA8060-35A-33-000 type has a footprint of 80 mm x 60 mm (vibration plate). At a frequency of 200 Hz (sine-wave) and a voltage of 24 V peak, the component offers a typical displacement of 55 µm. PiezoHapt is an ideal component for providing haptic feedback to user actions in the displays of smartphones and tablets.

The PiezoHapt actuator is a new addition to the lineup of TDK’s actuators with haptic feedback, which also includes the PowerHap series. Announced in November 2016, PowerHap types feature higher displacement and the highest acceleration and force, all in a single component with integrated sensor functionality, and are suitable especially for applications in vehicles, household appliances, game controllers, industrial equipment and more. With the new PiezoHapt and PowerHap product families, TDK can now provide cutting-edge high-performance haptic solutions for a very wide range of applications.

Main applications

  • Displays for smartphones and other devices, car navigation systems, touch pads, controllers, etc.

Main features and benefits

  • Low driving voltage of ≤24 V
  • Thickness of about 0.35 mm, making it one of the thinnest haptic devices in the world
  • Very short response time
  • Wide variety of possible vibration patterns

Key data

TypeDimensions [mm]Max.
operating voltage
[V]
Displacement
[μm] *
Operating temperature
[°C]
Vibration platePiezo element
PHUA8060-
35A-33-000
(commercial grade)
80 x 60 x 0.25 30 x 30 x 0.1 24 55 (typical) -10 to 60
  • * At 200 Hz (sine wave) without load

About TDK Corporation

TDK Corporation is a leading electronics company based in Tokyo, Japan. It was established in 1935 to commercialize ferrite, a key material in electronic and magnetic products. TDK's portfolio includes electronic components, modules and systems* marketed under the product brands TDK and EPCOS, power supplies, magnetic application products as well as energy devices, flash memory application devices, and others. TDK focuses on demanding markets in the areas of information and communication technology and consumer, automotive and industrial electronics. The company has a network of design and manufacturing locations and sales offices in Asia, Europe, and in North and South America. In fiscal 2016, TDK posted total sales of USD 10.2 billion and employed about 92,000 people worldwide.

  • * The product portfolio includes ceramic, aluminum electrolytic and film capacitors, ferrites, inductors, high-frequency components and modules, piezo and protection components, and sensors.

Downloads

Contacts for regional media

RegionContactPhoneMail
Japan Mr. Sumio MARUKAWA TDK Corporation
Tokyo, Japan
+813 6778-1055 pr@jp.tdk.com
ASEAN Ms. Jiang MAN
Ms. Pei Lu LEE
TDK Singapore (Pte) Ltd.Singapore +65 6273 5022 asean.inquiry@sg.tdk.com
Greater China Ms. Clover XU TDK China Co., Ltd.
Shanghai, China
+86 21 61962319 pr@cn.tdk.com
Europe Mr. Frank TRAMPNAU TDK Europe GmbH
Duesseldorf, Germany
+49 211 9077 127 frank.trampnau@eu.tdk.com
America Ms. Sara M. LAMBETH TDK Corporation of America
Irving, TX, USA
+1-972-409-4519 sara.lambeth@us.tdk.com

PAGE TOP