News Center | Press Releases

Temperature sensors: Lineup of high-precision IEC 0402 SMD NTC thermistors expanded

  • New 10-kΩ type features a narrow tolerance of ±1 percent
  • Optimally suited for temperature measurement and compensation in communication modules, mobile devices, and wearable devices
Temperature sensors: Lineup of high-precision IEC 0402 SMD NTC thermistors expanded

Mar. 31, 2015

TDK Corporation has expanded its NTCG04 lineup of IEC 0402 case size (EIA 01005) SMD NTC thermistors with a new type featuring a nominal resistance of 10 kΩ and a narrow tolerance of just ±1 percent. The new component complements the existing 100-kΩ type in 0402. With its miniature dimensions of just 0.4 mm x 0.2 mm x 0.2 mm, the NTCG04 lineup is optimally suited for temperature measurement and compensation of microcontrollers and displays in communication modules, mobile devices, and wearable devices.

The characteristics of the 0402 types are equivalent to those of the 0603 (EIA 0201) case size products, thus supporting the design of even smaller communication modules and increasing the mounting density in mobile devices. Achieving these ratings in a 0402 component was made possible by further optimizing both the source materials and the manufacturing process.

Mass production of the new NTCG04 type is scheduled to begin in July 2015. In future, the lineup of 0402 SMD NTC thermistors will be expanded with further nominal resistance values.


Main applications
  • Camera modules, LED modules, Wi-Fi and other communication modules
  • Mobile devices such as smartphones, tablets, headphones and microphones
  • Wearable devices
Main features and benefits
  • Miniaturized IEC 0402 case size (EIA 01005)
  • Nominal resistance of 10 kΩ and narrow tolerance of ±1 percent
Key data
TypeCase size
[IEC]
Dimensions
[mm]
Nominal
resistance R25
[kΩ]
Tolerance
[%]
B value
[K]
NTCG043* 0402
(EIA 01005)
0.4 x 0.2 x 0.2 10 ±1 3435 (25/85°C)
NTCG044* 100 4250 (25/85°C)
About TDK Corporation

TDK Corporation is a leading electronics company based in Tokyo, Japan. It was established in 1935 to commercialize ferrite, a key material in electronic and magnetic products. TDK's portfolio includes electronic components, modules and systems* marketed under the product brands TDK and EPCOS, power supplies, magnetic application products as well as energy devices, flash memory application devices, and others. TDK focuses on demanding markets in the areas of information and communication technology and consumer, automotive and industrial electronics. The company has a network of design and manufacturing locations and sales offices in Asia, Europe, and in North and South America. In fiscal 2014, TDK posted total sales of USD 9.6 billion and employed about 83,000 people worldwide.

  • * The product portfolio includes ceramic, aluminum electrolytic and film capacitors, ferrites, inductors, high-frequency components such as surface acoustic wave (SAW) filter products and modules, piezo and protection components, and sensors.

Downloads

Contacts for regional media
RegionContactPhoneMail
Japan Mr. Yoichi OSUGA TDK Corporation
Tokyo, Japan
+813 6778-1055 pr@jp.tdk.com
ASEAN Ms. Jiang MAN
Mr. Shota KANZAKI
TDK Singapore (Pte) Ltd.
Singapore
+65 6273 5022 asean.inquiry@sg.tdk.com
Greater China Ms. Clover XU TDK China Co., Ltd.
Shanghai, China
+86 21 61962307 pr@cn.tdk.com
Europe Mr. Frank TRAMPNAU TDK Europe GmbH
Duesseldorf, Germany
+49 211 9077 127 frank.trampnau@eu.tdk.com
America Ms. Sara M. LAMBETH TDK Corporation of America
Irving, TX, USA
+1-972-409-4519 sara.lambeth@us.tdk.com

Recommendations

PAGE TOP