News Center | Press Releases

TDK Booth at CEATEC JAPAN 2014

  • Building the Future with Magnetic Technology
TDK Booth at CEATEC JAPAN 2014

Oct. 3, 2014

TDK Corporation will be exhibiting at CEATEC JAPAN 2014, to be held at the Makuhari Messe from October 7 (Tue) to 11 (Sat).

"Building the Future with Magnetic Technology" is our booth slogan this year. TDK was founded on the magnetic material ferrite, and our exhibits will be focusing mainly on magnetic technology and the various applied products that we have created, as we continue to offer our technologies and products of their value to society.

We look forward to welcoming you at the TDK booth.

Outline of TDK booth and main products and technologies on display

Outline of TDK Booth
The starting point of this year's TDK booth is the "Magnetic Technology zone," looking back at the history of products based on ferrite which can be seen as the DNA of TDK. From there, the booth flow leads into three zones highlighting the latest applications of advanced magnetic technology: "Energy", "EMC" and "Data Storage & Sensors".

    1. Magnetic Technology zone
      Introduces magnetic materials (ferrite cores) are shown, which are in the DNA of TDK since its founding in 1935. The zone also illustrates the evolution of TDK's innovative product technology as it progressed along with the growth of the electronics sector in Japan.
    2. Energy zone
      Demonstrates how magnetic materials can enhance the transfer of energy and contribute to improved efficiency. Major highlights of the exhibit are listed below.

      - Wireless power transfer system for vehicles, etc.
      A wireless power transfer system for vehicles featuring sufficient reliability to allow for on-the-road testing (in terms of vibrations, load bearing, waterproofing etc.) will be demonstrated. A key architectural feature of this system is its magnetic resonance technology, for which WiTricity Corporation holds the foundational patents. Samples of a 3.3kW system will be made available from January 2015, and a 6.6kW system is also under development. Dynamic charging to transfer power to driving vehicles, and wireless power transfer systems for other applications will also be demonstrated.

      - High-performance magnets that help to conserve resources
      Exhibits include dysprosium free neodymium magnets, lanthanum and cobalt free ferrite magnets, as well as other products that illustrate TDK's commitment to realizing high-performance magnets that do not use rare earth materials.

    3. EMC zone
      The zone showcases EMC components based on magnetic materials, which are a specialty of TDK. Comprehensive EMC solutions ranging from anechoic chambers for noise measurement to devising suitable countermeasures will also be introduced.

      - EMC components
      - Anechoic chamber solutions
    4. Data Storage & Sensors zone
      In this zone, visitors will encounter TDK's cutting-edge spintronics technology based on magnetic materials.

      - HDD magnetic heads
      In the field of HDD heads which are a representative application of magnetic thin film technology, thermal assisted magnetic recording heads will be on display.

      - TMR angle sensors
      The thin film technology based on HDD heads has enabled TDK to develop magnetic sensors that can perform angle detection with high accuracy.

      - High-sensitivity magnetic sensors
      The exhibit provides a glimpse into the ongoing development of magnetic sensors that can detect even extremely weak magnetic fields.

      - MRAM
      The current state of development in the area of MRAM (Magnetoresistive Random Access Memory) which is an extension of spintronics technology will be introduced.

TDK booth location
Hall 5/5K111, Key Technologies Stage


About TDK Corporation

TDK Corporation is a leading electronics company based in Tokyo, Japan. It was established in 1935 to commercialize ferrite, a key material in electronic and magnetic products. TDK's portfolio includes electronic components, modules and systems* marketed under the product brands TDK and EPCOS, power supplies, magnetic application products as well as energy devices, flash memory application devices, and others. TDK focuses on demanding markets in the areas of information and communication technology and consumer, automotive and industrial electronics. The company has a network of design and manufacturing locations and sales offices in Asia, Europe, and in North and South America. In fiscal 2014, TDK posted total sales of USD 9.6 billion and employed about 83,000 people worldwide.

* The product portfolio includes ceramic, aluminum electrolytic and film capacitors, ferrites, inductors, high-frequency components such as surface acoustic wave (SAW) filter products and modules, piezo and protection components, and sensors.

Contact for media
ContactPhoneMail
Ms. Mari MIYAUCHI TDK Corporation +81 3 6778-1055 pr@jp.tdk.com

Recommendations

PAGE TOP